Other Parts Discussed in Thread: GPCRA0
Hi all,
I have a problem that Ra table has been updated large value after charge/discharge test, the failure is 11/80=13.75%. There are three phenomanon as below.
1. SOC 80% jump to 100% during charge.
2. After fully charge, I still charge pack many hours and found SOC 100% jump to 91%, and sometimes I remove charger the SOC went down, either.
3. SOC changed from 92% to 100% when I replug battery.
The update status=06 and calibration done before test. Mean while, I compared these packs and I found Ra table has been updated large value and Qmax smaller than good packs. And I do learning again, these packs problem is solve. What reasone may cause Ra table has been updated large value?