Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50, BQ28Z610, GPCCHEM
Hello everyone,
My setup is bq40z60 custom board with 3s Panasonic NCR18650B cells, Charging and discharging works flawlessly. Then, I try to complete the automatic learning cycle, and things go weird.
I had followed slua777.pdf cycle order:
4.2.1 Discharge Battery to Empty
4.2.2 Relax for 5 Hours
4.2.3 Charge Battery to Full
4.2.4 Relax for 2 Hours
4.2.5 Discharge Battery to Empty
However, I am stuck at different steps
1) If I start the learning cycle, it clears QEN bit. It is never set afterwards. So, after step 4.2.2, it cancel the cycle with a corresponding message. Relax time is also less than 5 hours (varies on different attempts, but I guess it's okay because RDIS is cleared).
2) If I try to bypass the issue with QEN bit and send GAUGE_EN command after having the cycle started, here's what I get. Step 4.2.2 is skipped (relax time is 00:00:00, the cycle goes right next to charging). Charging is done properly (FC bit is set), and relax time (4.2.2) ends with an error "VOK is not cleared". Looking in the log, it really never clears while relaxing.
What shall I do to make this cycle work? It is unclear what causes such failures.
I've attached the log file and gg.csv files:bq40z60_learning_cycle_fail.rar
Will be endlessly thankful for any help!
Best regards,
Michael.