LM5116 application is currently a problem, need to ask about
Ruv1 from 62K to 47K, Ruv2 is 16.9K, the combination of the pressure points as shown below
Vin range of products is relatively large range of 9V to 57V, such as the use of partial pressure calculation does not produce problems
But the test unit in the 57V test, it is easy to cause no output phenomenon
After verification is D1 burned or it is hot
Want to know, UVLO voltage level and D1 What is the relationship?