This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: BQ24650

Part Number: BQ24650

We have planned to use BQ24650 Battery charger controller in our design.

From solar panel input voltage, the BQ24650 is used to charge the battery as well as to source the load simultaneously.

The solar panel input power is connected to the External load and Battery at the same time, When the sun light is more the external load current will be provided the solar panel, as well as the remaining power will be be given to charge the Battery. When there is no sun light the load current will be provided by the battery.

 If solar panel input power not able to power full load that time remaining power to load can be shared by battery or not ?