This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5018: The simulation results of LM5018

Part Number: LM5018


Tool/software: WEBENCH® Design Tools

Hi

I simulated LM5018 under Vin=34~60V, Vout=5V and Iout=150mA.
I have two questions about the simulation results.
1. I could simulate I enter the condition in attached document① but I couldn't simulate if I enter the conditioon in attached document②.
   Could you tell me this reason?
2. The simulation result of the attached document② is used trance.
   Could I simulate the circuit using inductor?

Best regards,

Yokota