This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195: D+/D– based USB host/charging port detection

Hi,
I also don't need to use the USB host/charging port detection so I short circuited D+ and D- but it seems that the IC has an input current limit of 100 mA with Vsys equal to 1,7 V.

Update: now I have on Vsys the right value but I hear like a whistle: it seems that the internal loop compensation is unstable