Hello!
wanted to ask is there someone who can help me to design one power supply pcb:
i want to use an appropriate buck converter to transform incoming 14-24 DC and have dual output on +12V and -12V and also 5V (which will be via one regulator I imagine) so in fact will be triple output
all that with at least 900 mA or 1A or more at output (maybe less for 5V)
would like to be not bigger than 7cm X 4,5cm, with good efficiency and silent
if it that is possible i will be grateful for your kind help since I'm not an engineer (so not understand everything on webench application)
Thanks in advance!