Other Parts Discussed in Thread: BQSTUDIO, , GPCCHEM, GPCCEDV, EV2400
When selecting the bq34z100-g1 in BQStudio, there are warnings stating that the interface may not be stable. Indeed, I see such actions, particularity when reading Data Memory. Sometimes it takes 3-6 tries of "Read All" before the Data Memory array is filled.
I do not see the "GPC Packager" inside BQStudio. Will it run with my setup? If so, I would use GPCCHEM or GPCCEDV?
I want to characterize 2x NiMH cells at 1900mAh. If there is a close chemistry profile that already exists, I would take that.
Thanks,
...kevin