hi all,
See BQ77905 datasheet have bq77905 Device Configuration,For Example:
But cann't find the following device configuration, Please provide Configuration table, TKS!
Importantly, if I demand
OV=4.18; UVhyst=300mV; =35mV-40mV; OCD1 (Threshold) OCD1 (Threshold) =60mV-70mV; SCD (Threshold) =120mV;
OTD (℃) =65, then60℃ recovery
OTC (℃) =50, then45℃ recovery
UTD (℃) = -15,then -10 ℃recovery;
UTC (℃) =0, then 5℃ recovery
Which device is suitable for selection?