Hi all
Would you mind if we ask TPS4H160-Q1
<Question1>
The datasheet shows "Nominal dc load curren" is 2.5A.
Does it mean it is possible to use 2.5A per CH? Or total?
We think as follows;
I^2×Ron = 2.5 × 2.5 × 0.16=1W
So, as power dissipation, it prefers to be less than 1W.
As the result, 2.5A means total current value, right?
<Question2>
Is it possible to use ST pin as power good status?
<Question3>
About Fault pin, when it is satisfied the condition of any output fault, will this pin operate?
<Question4>
In case of events which corresponds to diagnostic fucntion, do each outputs stop?
– Overcurrent and Short-to-Ground Detection
– Open-Load and Short-to-Battery Detection
– Global Fault Report for Fast Interrupt
Kind regards,
Hirotaka Matsumoto