This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: Schematic review

Part Number: BQ25895


Hello

One of my clients is using the BQ25895 for this project.

It seems to me that it was applied with the right design values.

Could you please take one more review?

I will deliver the corresponding schematic file.

<<schematic deleted>>

  • Hi Andy,

    The schematic looks reasonable except for the 33ohm pull up resistor on INT. INT cannot sink more than 10mA. Also, please confirm that the inductor is rated for the highest of either charge current or boost mode input current from the battery using eff=VBUS*IVBUS/(VBATmin*IBAT).