This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A6950EVM: TPS7A6950-Q1:About the absolute maximum rating of the input current

Part Number: TPS7A6950EVM

Absolute maximum ratings of voltage are stated in TPS7A6950-Q1 datasheet.
  Vin:-0.3V(min)~45V(max)

Q1.
Could you tell me the absolute maximum rating of the input current?
Or, can you tell me how to think about it?

-Haurkawa