Other Parts Discussed in Thread: BQ51003
Hello,
I was testing the Bq500212A and BQ51003 EVM modules and was checking for the efficiency.
Following the Bq500212A EVM test procedure, I supplied 5V and 3A current limit at J1 and J2. After placing the BQ51003 EVM on it, the receiver is tripping with a blinking red LED after 200mA. Why is this happening?
I have set jumper JP3 from TS to EN and JP6 from ILIM to ADJ. R3 and R16 are set to 10kohm and 600ohm respectively.
Expecting this to be a procedure following issue, I started to follow the BQ51003 EVM and applied 19V and 1A current limit to the power supply of TX EVM (i.e., J1 and J2 pins). But, it stopped displaying D5 LED status now.
Now, my TX module does not switch on even with micro USB. Could you please tell me what is wrong?
Even though I am supplying 5V input, it is displaying 1.1V.
Thank you.