Hello,
My question concerns the LM5030 IC. In the application at hand I wish to measure the rectified and filtered output voltage of a transformer and regulate the duty
cycle applied to the primary (full bridge) as consequence.
By reading the datasheet it is not clear to me what the relation is between the VFB pin and the COMP pin. It would seem that the op amp that is inputed VFB and 1.25 V
works as a comparator, in which case the effect of the COMP pin is not evident.
On the other hand if the COMP pin is driven externally I do not understand what the effect of applying VFB is.
This is based on the figure at page 10 of the LM5030 datasheet.
I have also considered the different suggested/typical applications, but this has still not provided me with an answer.
Thanks
Gabriele Ulissi