Hi,
Could someone point me to specific application notes that deal with DC/DC (boost topology) power supply ripples attenuation?
My design is battery powered and consumes very low power, 90% of time stays in standby mode which consumes about 600uA, there are some spikes in running mode about 16mA. The input voltage is 3.6V, lithium battery and the design needed input voltage is 5.0V. Do you have any suggestions on what DC/DC convertors should I use?
Thanks,
Cristian