I am using a TPS79933 for a project. on the data sheet it appears that this should have a fixed output voltage of 3.3V. I have a couple of questions,
Is this the case that it is actually a fixed output voltage?
Is there a special configureation I need to apply to it to achieve this?
What are the packag markings that identify that it is actually a TPS79933?
I have it set up according to the discription below, and it is just tracking the input voltage, rather than supplying a constant 3.3V output. I.E. if I give a 3V input, it is giving a 3V output, if I give it a 4.5V input, it has a 4.5V output.
pin ->10 uF and .1uF capactior fromto ground (Vin)
pin 2 -> ground (GND pin)
Pin 3 con-> same node as pin 1 (ENABLE PIN)
Pin 4 ->.1uF cap to ground
pin 5 -> 2.2uF cap to ground with a 470k resistor to provide a load.