Hello guys,
One of my customers is designing a schematic for their product uses UCC28950. They have several questions about SYNC terminal as the follows. Could you please give me your answer or comment to the questions?
Q1. What is the SYNC terminal maximum driving current when the terminal works with output mode?
Q2. What is the threshold voltage when the terminal works with input mode?
Q3. What is the maximum voltage which can applied to SYNC? Is it 5V?
Q4. What is the minimum voltage which can applied to SYNC? Is it 0V?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.