Other Parts Discussed in Thread: TPS54339
Can TPS54339E make this application?please help confirm.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cheng,
Yes, you could use to create inverting voltage. But need to remember that, in this application, the GND pin of TPS54339 is connected to FB-5V, which means that all the other pin is reference to FB-5V as GND. In this case, SS cap, VREG5 cap and EN pin should reference to F-5V not board ground. Please consider this in this kind of application. Other than that, please also put one or two input cap between Vin pin and GND (Fb-5V) pin of IC. Thanks!