This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A: bq76pl455a

Part Number: BQ76PL455A

hi 

i have one question about bq76pl455a, which is support stack 16 IC, it's mean it is support maximum voltage is 3.6v*16*16= 921V; if our system is higher than 1000V, is BQ76PL455A still suitable for us?

because we want used for our high voltage ESS. if it is still suitable, how to do it?

  • Lina,

    How many cells/ modules are you wanting to stack?

    You are correct about our 16 module limit. There may be other ways to work around it - such as using a "hybrid" architecture with 2 base devices and 2 daisy chains. With some creative part selection/schematic design this can be done with one MCU