Other Parts Discussed in Thread: BQSTUDIO, BQ76930, , EV2400
Tool/software: TI C/C++ Compiler
I designed a board, using BQ78350-R1 and BQ76930 to manage 8 sets of batteries, and the battery uses a lithium titanate battery. Board connected to EV2400, using BQStudio tool to debug. Because the battery is not conventional, the default configuration of the chip and the measured values are wrong. some configuration need to be modified. Is there a detailed chip debugging document? For example, what registers need to be modified first, then voltage, current calibration, battery capacity, self learning, GPC.
After I changed a few parameters, the voltage and current are measured correctly. But the percentage of the remaining capacity is shown wrong (display 0% for full battery). I don't know how to solve.