Other Parts Discussed in Thread: BQSTUDIO, , EV2400, BQ34110
Hi,
I have just purchased a BQ34110EVM-796 and EV2400 and I am now trying to bring up the system using bqstudio v1.3.54.1 on a Win10 PC.
As bqstudio starts it detects the device as bq34110 as 0110_0_02, but this device is not listed as a supported target device, the closest part is 0110_0_01-bq34110.bqz.
Surely this latest version of bqstudio should support this device?
Selecting 0110_0_01-bq34110.bqz as the target device, I can then start bqstudio with a warning, however I am now having problems setting up the device configuration correctly.
I am using a 2 cell series Li-Ion pack, I have set un-seal full access mode, Set CAL_EN and VEN_EN bits and set the number of series cells to 2. When performing "write_all" I get the following error "Value is beyond maximum value defined for parameter:Safety.BATHIGH.Battery Hugh Set Threshold"
The battery voltage on the dashboard is showing 2154mV when the actual battery pack voltage is 8.27V. Measuring VEN pin from the bq34110 shows that it is not set HIGH.
Any ideas what I am doing wrong?
Thank you