Other Parts Discussed in Thread: LM25118
Hello,
Could you please answer a question from my customer.
He is trying to implement WPT for a lighting application.
the bq51025 is not going back into the 10W after I created the over temperature stop and stays in the 5W mode.
I also just found another problem. When the LM25118 is turned on. The wireless charging is not working anymore. I could see 2 things. The first I saw, that the charging was starting but my LEDs are flickering and the charging stopped after very few seconds. This behavior repeats than. The second thing I see is when the LEDs are running and I power up my charger the charging tries to start and then stops. It seems that the charger is communicating with my device but no power transfer happens. If after some time the power transfer starts the LEDs are starting to flicker again bevor the charging stops.
Thank you in advance.
Best,
Needhu