This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C23DEVM-807: TPSM846C23DEVM-807

Part Number: TPSM846C23DEVM-807
Other Parts Discussed in Thread: TPSM846C23

Hi

With regard to the TPSM846C23DEVM-807 that I purchased for testing, it did not come with a USB-GPIO cable to interface with the Fusion Power Designer software.

On the Eval board, there are two resistors each connected to the FB pin of the two devices in parallel.

Is it possible to change the default Vout = 0.6V to Vout = 1.8V by replacing resistors or can this be done only via software program? If so, should I be replacing both resistors connected to FB pins of respective devices in parallel or one of them?

Please advise 

Thanks

Rony Kuriakose