Dear all,
Could I change threshold of the VRCH(Recharge threshold voltage)? Or, could I change Vset lower at fully charged and change it higher at the target voltage that I want to use.
I would like to use battery until lower voltage after fully charged.
For example, I would like to use the battery as Vset = 4.35V and the voltage to start recharging = 3.88V. However, if VRCH is fixed 120mV, this device will recharge at 4.23V. This is out of need.
If I can change Vset = 4.35→4.0V at fully charged, I can use battery until 3.88V. And if I can change Vset = 4.0→4.35V at 3.88V, I can fully charge the battery.
Could I use either way?
Best regards,