Other Parts Discussed in Thread: TPS715
Hi,
My customer has a question.
Q1.
I am checking whether the rise and fall times of the IC are correct.
Are the following rise and fall times appropriate?
TPS7A4901
[Using condition]
Vin: 27.7V
Vout: 21.6V
Iout: 0A
Csoftstart: OPEN
Cout: 28.9uF
Startup time: 600us
Shutdown time: 96ms
TPS71501DCKR
[Using condition]
Vin: 4.98V
Vout: 4.11V
Iout: 0A
Cout: 1.2uF
Startup: 130us
Shutdown: 165ms
Q2.
In order to check if it is reasonable time,
Do you have materials like evaluation data?
(TPS71501 was described in the datasheet (page12)
TPS7A4901DGNR didn't have described.)
Q3.
The TPS7A4901DGNR is controlled by the EN pin.
From the timing when EN is turned OFF,
How long will it take for the OUT to start falling?
Best Regards,
Watanabe