Hi,
I know that the bq25703A EVM use 10uF x6 as input capacitor, and the EVM can be used for 3.5V to 24V / 6Amax adapter. But now the customer design their system with only 5V / 1.5A adapter for 2s1p battery. Then can you recommend the 4.7uF or 4.7uF x2 as input capacitor for 5V / 1.5A input source for 2s1p battery?
Best Regards,
Satoshi / Japan Disty