Other Parts Discussed in Thread: BQ76940, GPCCEDV
Hello to Ti team ,
I am working now with bq78350-r1 & bq7694001 , my questions are.
1. Is it necessary to connect cells to AFE in order : 1. 1N 2. 1P 3. 2P ...... ?
2. How I can influence to reduce max error from 100% to 1% ? , Is there any tutorial about it .and any risk produce battery with max error 100% ?
3. Is it necessary use GPCPAckager for high accuracy ? , If i don't have time to prepare this 6 flog files what should be estimated error in RC ?
4. I use chemistry with is out of chem list : ICR18650-26JM , can you please advice me with chemistry use instead with close parameters .
5. I can't find Gauge Enable option like in 40z50 ,20z655 , How i enable Gauge ( start Algorithm and lifetime logging) ?
Thanks in advance
Electronics Design Engineer.
Alex Burtakov