Other Parts Discussed in Thread: LM2676
Tool/software: WEBENCH® Design Tools
Dear Sir, please, answer
I use LM2676, please, see attach. Ripple on the out sometimes arises. And sometimes there is no ripple. I shot the oscillograms. If there is a ripple at the output, then the pulses at VD1_L4 are distorted at the front. If there are no ripple, then the pulses at the VD1_L4 are not distorted. L1 and L5 - are ferrite beards. PSB is two-layer.
L5 is now off. Output current 1.8- 2.0A - I connected external load. If the out current is less than 1.7 A, then there is no ripple, but I need it to be 2 A.
I added two oscillograms of 'bad" ang "good" pulse on VD1_L4. And and also, please, see the packed files
TIA
Sincerely
Vladimir NaumenkovLM2676SX.RAR
www.agat.by