Other Parts Discussed in Thread: TPS62097
Dear *,
i want to use the TLV62568 for supply a core from other FPGA IC and the core is decoupled with 1x100uF or 1x47uF, 5x10uF and 10x100nF.
The output LC of the TLV62568 is described in table 4 in the DS and it says that we should use 2.2uH inductor and 2x22uF capacitor for stability (1V output).
What is the maximum capacitance load for this DC/DC?
If we load the switcher with the additional sum of 100uF + 5x10uF =~ 150uF how can i simulate the stability with TINA?
Best Regards.