is providing 3.3 v on the ENABLE PIN and avoiding the UVLO feature can harm the device
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS54020 does not require use of the external UVLO function. EN is internally pulled up. TI recommends to use open drain or open collector logic. That said, the abs max voltage for EN is 6 V, so 3.3 V should not damage the IC.