This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54A20: About bode plot of TPS54A20?

Part Number: TPS54A20

Dear support member,

My customer created TPS54A20 board and
Bode plot measured.

Looking at the measuerement Bode plot,

DC gain was 1kHz of 24dB.
Cross over frequency was 2MHz, phase margine was 39 degree.


Looking at the Datasheet Fig52,
DC gain was 1kHz of 55dB.
Cross over frequency was 300kHz, Phase margine was 45 degree.

Could you say that the measurement bode plot correct from the above contents?

Best regard.

Bob Lee