This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A90: TPS7A90: Please suggest R1 and R2 values for 1.8v,2.0V,3.6V and 4V

Part Number: TPS7A90


Hi

I need to provide an option for multiple output voltages(1.8,2.0,3.6,4.0) with 500mA current from 3.5-5V input voltage

For this purpose I chosen TPS7A90 is this better choise(0.6mV rms noise on output voltage) ?

can you please suggest R1 and R2 values for 1.8V 2.0V 3.6V,4V outputs

Regards

Sukumar Reddy