Hi,
we have designed a converter using the LMR64010 but only get approx. 220 mA but not 300 mA.
If we go below 60 Ohm load, the output voltage starts to break down. For example:
59 Ohm 11.8V 200mA
55 Ohm 11.5V 209mA
47 Ohm 10.8V 229mA
31 Ohm 8.5V 274mA
We have followed the layout recommendations in the data sheet.
Diode: MBR0520
Inductor: ABRACON ASPI-2010HC-100M-T
Any advice is welcome?