Dear Support team
We have questions about start up (8.4.11) and shutdown sequence(8.4.12).
(1)What is the transition trigger from Device INIT state to STAND BY state ?
(2)How long is the time (max) from triggering to transition?(raugh time is helpful for us,not need gurantee)
(3)How long is the minimum time (or PWM cycle number?) required from the start of PWM input until EN High in start up sequence?
(4)How long is the minimum time (PWM cyc number?) required to stop PWM input from EN Lo in shutdown sequence?
(5)About shutdown sequence, please tell me the behavior if not maintain 400 ms of DISCHARGE period and power-off.
Sorry for many questions.
Regards
Tomohiro Nagasawa