Dear e2e Community,
My customer uses our HV LDO in this configuration:
- Vin = 90V DC
- Vout = 84V DC
- Iout = 10-20ma peak
The issue is about the distance between Vout pin and VFB pin. Due to the package, this distance will be in worst case : 0.27mm (0.65-0.38)
The Standard regulation (IPC-2221B) requires that the minimum spacing between 2 conductors should be 0.6mm if the voltage difference is around 80V
Questions
- What would you suggest in order to safely use the TPS7A4001 in this configuration ?
- Could we say that even if the local spacing between VFB & VOUT is thin, the possible leakage current will still be neglectable compared to the current going through the resistor network divider ?
Regards,