Other Parts Discussed in Thread: TLC5941-Q1
Hi All
My customer is trying to use it under the following conditions.
VLED = 16 V
Iout = 40 mA/ch
Temp MAX = 80 ° C
Number of LEDs: 15 para
Number of channels = 15 ch
When calculating the maximum allowable loss, 0.9 W @ 80 ° C. (150-80)/78=0.9W
40 mA * (16 - Vf) V = 7.8 W @ Vf = 3
It will exceed the maximum allowable loss.
We are trying to add a resistor as a countermeasure.
How is it correct to calculate the resistance value?
Best Regards,
Koji Hayashi