r: TPS28225
Dear,
Attached you will find a schematic of a TPS28225 based design, used as a constant current source. Vin 25..26Vdc, Vout 0..24dc, Iout 0..10A. Controlled by using a 226kHz PWM signal. Feedback to a microcontroller by voltage and current measurement.
The schematic shows a 5V supply voltage to the TPS28225, in reality this is 4.8V. This voltage is not ideal but it works at the customer.
The design works well, having a 6.8 Ohm load connected to the output. By using a 226kHz PWM signal the output can be set between 0 to 24V, with a current between 0..3.5A. When doubling the output current (so the load is 3.4 Ohm) the TPS28225 starts to smoke at 10% duty cycle (output voltage is around 3V than). So the TPS28225 gets burned.
Normally I would expect the T7 and T8 to be burned when the current gets too high,but not gate driver.
Questions: Can you explain this? Could the be related to the bootstrap capacitor / circuit. See a Fairchild application note as well (attached in the zip file). Or what else could cause this problem?
Are there any good other reference to build a constant current source, based on this device?
Thanks in advance and kind regards,
Wim van der Steeg