Tool/software: WEBENCH® Design Tools
Hoi guys,
For my school project I have used the LM25118 to convert 9-36 VDC to 12 VDC 2A. With the help of Webench I have built a circuit. But it doesn't work as I hoped.
When the input was 14 VDC, first the voltage at the negatief side of the conductor (V_conductot_ground) was 12 VDC(square wave). But when I tried to measure the output voltage, I don't get 12 VDC but a strange signal. the output voltage was less dan 1 V DC. After that I have measured the V_conductor_ground) again but the square wave of 12 VDC is gone, in place of that is a strange signal. Can someone explain me why?.
I have used the circuit below and the VCCX is connect with the ground.