Just want to know which part can give us a smallest solution for a 5V 2A battery charger. The input voltage is 100-240V 50/60Hz.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jiwei,
Thank you for posting.
PMP8286 on TI.COM is a perfect small size solution for a charger.
This reference design uses the UCC28700 in a quasi-resonant flyback to generate an isolated 5V at up to 2.1A. The UCC28700 implements primary-side regulation, eliminating the need for an opto-coupler and reducing the total component count. This results in a compact and cost effective design. The populated circuit boards in this design occupy the space of a 1" by 1" by 1" cube. The TPS2511 USB power switch also offers the data line control to charge most smart phones and tablets. The energy saving features of the UCC28700 allow this design to consume less than 30mW when plugged into the wall with no device attached to the USB port.
All materials for creating this design are available at the link.
This design hardware is not available for purchase.
Here is a picture of what it looks like;
If this answers your question please confirm with the THIS RESOLVED MY ISSUE button.