This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A-Q1: Byte Position for data for Vmodule bytes

Part Number: BQ76PL455A-Q1

Hi 

for the IC i have channel configuration registers setup as 0xFFFFFFC2. I have also enabled the bit to get module voltage in test config register. Data sheet says that the  module voltage would be sent along with the command. What i am not able to figure out is what would the position of the module voltage be in the byes.

As i understand the data would come in as Cell16(lsb then MSB) CEll 15, 14 so on and so forth. Since i have temp and die channals enabled , aux data would be following the cell data and internal die temp would be following that. This is what i get WITHOUT the vmodule bits enabled in test config and channel registers. Where would the data for Vmodule be after i enable them. Would it still come as LSB first and then MSB like other data?

Thanks

Regards

Saurabh