This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Error in GPC Report

Part Number: BQ34Z100-G1


Hello,

I have sent data in per SLVA725 and here is the error report:

From File: GPC_Report.txt

       0 0
Error: Wrong data format  make sure file has coma or tab separated values. Name: roomtemp_rel_dis_rel.csv

From File: MiscInfo.txt

ProcessingType= 2

my config.txt

ProcessingType=2
NumCellSeries=2
ElapsedTimeColumn=2
VoltageColumn=9
CurrentColumn=10
TemperatureColumn=12

Sample from: roomtemp_rel_dis_rel.csv

Tue Oct 03 10:43:20 PDT 2017

Device Name = bq34z100G1
Firmware Version = 0_16


Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,LearnedStatus,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus
1,2017-10-03 10:43:32,11.272,0x0000,0x4000,2,100,1,64,2526,390,113,24.9,65535,35,0,493,25.3,6,0,4500,960,0x01D9,0x1116,0x0400,16,0,0,0,1,63,4,62,21,16384,0,-1560,1879,895,SUCCESS
2,2017-10-03 10:43:40,20.001,0x0000,0x4000,4,100,2,64,2590,391,241,24.9,65535,23,0,506,25.2,6,0,4500,960,0x01D9,0x1116,0x0400,16,0,0,0,2,63,13,61,21,16384,0,-1561,1879,887,SUCCESS
3,2017-10-03 10:43:52,31.268,0x0000,0x4000,5,100,3,63,2746,663,413,24.9,65535,15,0,910,25.3,6,0,4500,960,0x01D9,0x1116,0x0400,16,0,0,0,3,63,24,60,21,16384,0,-1562,1879,881,SUCCESS
4,2017-10-03 10:44:00,40.001,0x0000,0x4000,8,100,5,64,2788,647,514,24.9,65535,12,0,900,25.3,6,0,4500,960,0x01D9,0x1116,0x0400,16,0,0,0,5,63,33,58,21,16384,0,-1564,1879,884,SUCCESS
5,2017-10-03 10:44:12,51.266,0x0000,0x4000,12,100,7,63,2822,634,584,24.9,65535,11,0,895,25.3,6,0,4500,960,0x01D9,0x1116,0x0400,16,0,0,0,7,63,44,56,21,16384,0,-1566,1879,898,SUCCESS