Hi all
Would mind if we ask TPS1H000-Q1?
It's relation with follows post,
https://e2e.ti.com/support/power_management/switches/f/949/t/629444
Our customer wonders if it is possible to be filled with TPS1H000-Q1 or not.
Our customer's current condition : 6A, 20us
We guess that TPS1H000-Q1 can not be filled with specific because of follows;
-ICL(int) Internal current limit : NG(1.8A max)
-The fast-trip response time is less than 1 µs : NG(20us flow)
However, we have guestion about "Deglitch time when current limit."
<Question>
During tCL(deg), do "the device ICL(int) Internal current limit" and "The fast-trip response time is less than 1 µs" become invalid?
On the datasheet P10 Figure 9. Holding Mode Example, after tCL(deg) term, VFAULT outputs.
So, if you have some comment, could you let us know?
Kind regards,
Hirotaka Matsumoto