Hi Team,
I am reading through the TPS92515-Q1 datasheet, section 8.3.11. In section 8.3.11.1, it details how to apply a PWM signal to the PWM pin for dimming. Then, in section 8.3.11.1, it sounds like the PWM pin can be used either as a PWM input for dimming OR to adjust the hysteresis on UVLO level.. am I understanding that correctly? If not, can you please explain? If yes, then I can apply a PWM signal to that pin for dimming and adjust the UVLO levels at the same time?
In section 8.3.11.1.1, it explains how the resistor divider sets the UVLO lockout level, and section 8.3.11.3 explains that there are three pins where UVLO levels are applicable. Does the change in UVLO level due to resistors as described in section 8.3.11.1 cause a change in UVLO on all 3 pins? If not, where is the change in UVLO with the resistors applied?
Thank you in advance for the help!
Jared