This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6C5712-Q1: PWM fault always present,fault value readed is 0x3F

Part Number: TLC6C5712-Q1


Hi,

I'm using chip TLC6C5712-Q1 and Im having this issue with the PWM inputs, always getting a fault reported by ERR PIN coming from ANY_PWM_ERROR register. when i read the FAULT REGISTER i get the value 0x3F, that is; a fault is present for all PWM inputs, even if I mask some of them I still get this value and the error.

The only way to  not get this fault is by masking all of the PWM inputs, already checked the signal which is at 200Hz , it is Active Low as specified in datasheet and also the duty cycle time is nowhere near the limit, same with off time.

Is there anything else that can be triggering this fault?