Other Parts Discussed in Thread: UCC28700
Tool/software: WEBENCH® Design Tools
Hi ,
I am wondering if webench can use for design isolation power with more than one output voltage.
Now I am thinking about to design a flyback with 85 to 260 input range with following output
+15V@1A / REGULATION: 2%
+15V@0.3A / REGULATION: 8%
-15V@0.2A / REGULATION:8%
+24V@1A / REGULATION:8%
can UCC28711 meet this requirement and what should be concern when choosing the other parameter(resistor) when design system?
Thanks for your help.