This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54218: Stairlike output during starting-up

Part Number: TPS54218

TPS54218

For my DC/DC converter to generete 3.3V from 5V, I applied TPS54218 referenced the schematic shown in the User's Guide (SLVU331, Figure 16) with the following modification.

My circuit shows starlike output voltage, rampup to around 2.5V and stay there for about tens of mili-seconds (sometimes a couple of minutes), then go up to 3.3V.

Are there anyone who have the same phenomenon as above?  Could someone tell me why this happens?

<Modified devices from the original circuit stated in Fig.16.>

R3:11.5kohm

C1:10uF

C4:5600pF

C5:68pF

R7: 10kohm

R8+R6:31.1kohm,

C8,C9: 47uF each

C7: 0.015uF

EN: at Vin > 4.1V