This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650830EVM-095: Question about evaluation board schematic.

Part Number: TPS650830EVM-095


My questions refers to document SLVUAD6 which is the user guide for the TPS650830EVM-095. The schematic on page 5 shows pin G12, FBVR2N, connected to a 100 ohm resistor, R22, and then to the ground pin of the output capacitors. Why is that resistor value 100 ohms and not 0 ohms? The rest of the resistors in the feedback paths are 0 ohms.