This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Access Manufacturer Data with sealed battery

Part Number: BQ34Z100-G1

Hello, 

Can the manufacturer's data be accessed with a sealed battery? Class : Configuration. Subclass : Data.

Our customer would like to access data like: Manufacture Date / Serial Number / Device Name / Device Chemistry / etc. (Like BQ20z95).

Because if I understand correctly, all the data flash is blocked in reading if the component is sealed (except Manufacturer Info - Block A[1...31] ).

Waiting to read you,

Best Regards.

  • hi Charles,

    The data sheet says the manaufacturer info block in accessible in sealed more. Serial number is accessible in sealed mode -there is a command for reading this. device type and chem id is accessible in sealed mode as well. See table 2 in the data sheet. Manufacture date can be place in the manufacture info block to make that accessible if it isn't accessible in its default location. You can easily test that.

    thanks
    Onyx