I am in the process of completing a LiPo battery powered design and intend on using one of these ICs (BQ20Z95 or the BQ20Z75-v180) for the purpose of gas gauging and 1st and 2nd level protection (I do not require any of the charging features).
My questions are:
1. As the LiPo battery is the sole power source for the design, by simply pulling the SYSTEM PRESENT pin to ground (via an POWER switch on the design) when turning on the device with the LiPo battery connected, will I be able to enter discharge mode and hence power my design? (I am doubtful as I keep reading that an external power source is required to turn on the IC...)
2. Just to double-check, *PULL-DOWN* (not pull-up) resistors to ground are required at both ends of the SM bus (at the MCU and at the battery management IC). Correct?
3. Is the the LED display feature the only main difference between the BQ20Z95 and the BQ20Z75-v180?
I'd really appreciate it if anyone with experience with these ICs could help me answer these questions.
Cheers,
Nick