Hi guys,
Customer has a question with the BQ76PL455A:
I have a question on communication timing. For the various command and response messages, what is the response time of the BQ part? I’m creating a USB to BQ communication adapter and would like to add some timing circuitry to the communication path. We’ve implemented the communication in a similar to fashion to what has been described in the BQ use-case document, using CAN transceivers to send the UART information to and from the processor to the BQ. I’d like to add a RX block circuit to prevent RX action from happening while the TX is going on. Knowing the response rate can help me tune a circuit to that minimum response time.
On the BQ76PL455_GUI application that TI provides, is software compatible if it sees an echo when the application transmits a message to the BQ part? This is related to the above question.
Thanks,
Brian